Skip to main content

Overview

All copy, cut, and paste functionalities are available in the Ladder Editor through the Edit menu or the corresponding keyboard shortcuts. To perform these operations, you must have a rung or an element selected.

Copy/Paste an Element

Below is an example of copying/pasting an element.

Figure 1 - Before, element selected and pressing Ctrl+C

Figure 2 - Target insertion point selected

Figure 3 - After pressing Ctrl+V

Copy/Paste Multiple Elements

You can also copy, cut, and paste multiple elements selected by the mouse or the G key. Below is an example of copying/pasting multiple elements.

Figure 4 - Before, group selected and Ctrl+C pressed

Figure 5 - After, timer selected with previous insertion point and Ctrl+V pressed

There may be situations where pasting is not possible, with no change to the rung after the command.

Copy/Paste of Rungs

Rungs are selected for copy, cut, and paste operations using the mouse only, as shown in the following figures.

Figure 6 - Using the mouse, from the outside right of the rung

Figure 7 - Using the mouse, from the left side of the rung

It is also possible to select multiple rungs for these operations.

The following is an example of copying/pasting a rung.

Figure 8 - The rung to be copied is selected and Ctrl+C is pressed

Figure 9 - The rung immediately above the selected paste

Figure 10 - After pressing Ctrl+V