Skip to main content

Export - Configuration and Binaries

WPS has three export options available in the File > Export menu:

  • Read parameters and export
  • Export configuration
  • Export Binaries for Download

Read parameters and export

This feature creates a configuration, backs up parameters and logs (if available), and stores them in a backup file (extension .bkp). It requires a device connected to the computer for the information to be read.

The first step is to configure the configuration to establish communication with the device.

Communication Configuration

Note: If there is no communication with the device, a message will be displayed and will interrupt the data export.

Error - No Device

When you confirm communication with the device, a window will appear for selecting the automatically created resource.

Creating Project

Select the resource and click Next.

Select Resource

Wait for the data to be read.

Note: Depending on the selected communication type, this process may take a few minutes.

When the data is read, a summary of the acquired information will be displayed. Click Next.

Export Report

The configuration information is displayed. You can modify the configuration name. Click Finish.

A folder containing the configuration file will open after this step is completed.

Configuration Backup

System folder containing the generated backup file:

Backup File Location

Export Configuration

To export the configuration to a backup file (.bkp extension), click Next.

Export Backup

Next, you can select the configuration resources to be exported. Click Next.

Select Resources to Export

The configuration information is displayed. You can modify the configuration name. Click Finish.

A folder containing the configuration file will open after this step is completed.

Finish Export

Export Binaries for Download

Creates a backup of binary files with the .bbp extension.

In the first step, you must select the Configuration. Click Next.

Export Binaries - Configuration Selection

Next, select the resource within the previously selected Configuration and click Next.

Export Binaries - Resource Selection

Select options if necessary and click Next.

Export Binaries - Options

The backup information is displayed. You can modify the file name. Click Finish.

A folder containing the backup file will open after this step is completed.

Finish Binary Export