Skip to main content

Importing Special Versions

1) Button/Menu Item — Import Special Version

In the Tools menu, click Import Special Version.

Import Special Version

2) Window — Import Special Version

A window will appear to import the database for the special version of the selected product.

Import Special Version Window

3) Database Import (XML)

Click ... and select the XML file previously provided.

Import Database (XML)

4) Custom Firmware Version Setting

After selecting the XML file, set the firmware version of the database to be imported.

Special Firmware Version Setting

Note: The database import process will not complete if the XML file is incompatible or corrupted.

5) Base Firmware Version Selection

Choose the firmware version provided by the database vendor to use as a reference. Click OK to complete the import.

Base Firmware Version Selection

6) Completing the Import Process

When the import is complete, a message appears in the Output window. After clicking OK, the WPS will restart.

Import Process Completion

7) Import Problems

ℹ️ Note: The database import process will not complete if the XML file is incompatible or corrupted.

During step 3, if the file is not compatible, the Output window will display an error message.

Import Problems - Error 1

After clicking OK, a message will appear stating that the database was not imported.

Import Problems - Error 2

To perform step 4, it is important to use the firmware version format compatible with the product. In case of inconsistency, an error message will be displayed.

Import Problems - Error 3