WPS V3.00
Functionalities:
| • | Included CFW900 V1.00.xx; |
| • | Included CFW700 v2.3x; |
| • | Included CFW500 v3.6x; |
| • | Included CFW300 v3.0x; |
| • | Included CFW100 v4.1x; |
| • | Included RUW100 v2.0x; |
| • | Included MW500 v3.0x; |
| • | Included WCW2200 v2.2x; |
| • | Included WECC300 v1.1x; |
| • | Included WECC300 v1.2x; |
| • | Included Enterprise v1.0x; |
| • | Included SIW600 v2.6x; |
| • | Included SIW600 v2.7x; |
| • | Included SIW700 v2.2x; |
| • | Included SIW750 v1.1x; |
| • | Included MVW-01 v3.0x; |
| • | Included MVW-01 v3.2x; |
| • | Included MVW-01 v3.3x; |
| • | Included MVW-01 v3.4x; |
| • | Included MVW-01 v3.5x; |
| • | Included MVW3000 v1.1x; |
| • | Included MVW3000 v1.2x; |
| • | Included MVW3000 v1.3x; |
| • | Included MVW3000 v1.4x; |
| • | Included SSW7000 v1.1x; |
| • | Included SSW7000 v1.2x; |
| • | Included SSW7000 v1.3x; |
| • | Included SSW7000 v1.4x; |
| • | Included SSW7000 v1.5x; |
| • | Included SSW7000 v1.6x; |
| • | Included SSW7000 v1.7x; |
| • | Included RTD v2.7x; |
| • | Included RTDW v1.0x; |
| • | Configurator and download DriveScan to CFW900; |
| • | Enhancement in conversor WLP to WPS; |
| • | ECW500 Status Wizard; |
| • | PSRW 1.1x Wizard; |
| • | CFW500 firmware download; |
| • | MW500 firmware download; |
| • | Event log for WCW2200; |
| • | WECC300 firmware download; |
| • | Parameters exporting; |
| • | It shows datatype in table parameters; |
| • | It allows to import device's version (Ve's); |
| • | Trend: current sampling rate, pause option, it allows you to monitor more channels. |
Enhancements:
| • | Trend: fixed zoom adjustment, performance improvement. |
WPS V2.60
Functionalities:
| • | Included ADW300 v1.00+; |
| • | Included CFW-05 v1.00+; |
| • | Included CFW-07 v2.00+; |
| • | Included CFW-08 v1.00+; |
| • | Included CFW-09 v1.20+; |
| • | Included CFW-09PM v10.00+; |
| • | Included CFW-11 v6.00+; |
| • | Included CFW-11M-G2 v1.10+; |
| • | Included CFW-11RB v1.10+; |
| • | Included CFW300 v1.00+; |
| • | Included CFW-300-2 v2.00+; |
| • | Included CFW700 v1.00+; |
| • | Included CFW701 v1.10+; |
| • | Included Corporate v1.00+; |
| • | Included CTW-04 v1.00+; |
| • | Included CTW900 v1.00+; |
| • | Included ECW500 v1.00+; |
| • | Included FAW700 v1.30+; |
| • | Included MVW-01 v1.40+; |
| • | Included MVW3000 v1.00+; |
| • | Included RUW100 v1.00+; |
| • | Included SCA-04 v1.00+; |
| • | Included SCA-05 2.10+; |
| • | Included SCW100 v1.00+; |
| • | Included SIW600 v2.50+; |
| • | Included SIW700 v1.80+; |
| • | Included SIW750 v1.00+; |
| • | Included SSW7000 v1.00+ |
| • | Included SSW900-CETH-W v1.10; |
| • | Included WCW2200 v1.10+; |
| • | Included WECC300 v1.00; |
| • | Added wizards option; |
| • | Added Firmware's Dowload; |
| • | Implemented Trace for MVW3000; |
| • | Added blocks at ladder: MW_SRAMP and MW_Stop2; |
| • | Implemented Force I/O for CFW100. |
Enhancements:
| • | Enhancements in the Communication Manager - WComm; |
| • | Corrections at manual; |
| • | Enhancements in compiling tasks; |
| • | Enhancements in solving theTrace; |
| • | AddedModbus address in the ladder tooltip; |
| • | Enhancements in the search tool. |
WPS V2.50
Functionalities:
| • | Included CFW500 V1.10+; |
| • | Included CFW501 V1.30+; |
| • | Included MW500 V1.50+; |
| • | Included CFW-11 V1.00+; |
| • | Included SSW06 V1.30; |
| • | Included SSW07 V1.20; |
| • | Included SSW08 V1.30. |
Enhancements:
| • | Corrections in the manual (help). |
WPS V2.40
Functionalities:
| • | Configuration Wizard for CFW300, PSRW, SSW900; |
| • | Main signal monitoring window's - CFW300, SSW900; |
| • | CALL block for PLC300 since V3.41 and V4.11 (according to hardware model); |
| • | USB driver enabling communication with PSRW; |
| • | Enhanced search system (includes search by blocks, indexed variables, texts). |
Improvements:
| • | Corrections in the manual (help); |
| • | WComm (communication manager supporting FTP protocol); |
| • | WEG USB driver supports Windows 10 (x86 and x64) - including build 1607 or newer; |
| • | New markers addresses for setting up HMI LEDs (PLC300 V4.1X). |
WPS V2.30
Functionalities:
| • | Included CFW300 V1.0X and V1.2X; |
| • | Included PLC300 V3.3X; |
| • | Windows 10 support (x86 and x64); |
| • | Automatic installation of the WEG USB driver; |
| • | Automatic installation of the FTDI driver; |
| • | Welcome window with quick access to some functions; |
| • | Improved communication configuration. |
Improvements:
| • | Improved performance and trend graph interface; |
| • | Improved organization of menus. |
WPS V2.20
Functionalities:
| • | Function to remove unused variables |
| • | Function to search and replace variables in the resource |
| • | Variables filter option inside the variables table |
Improvements:
| • | JRE (Java) embedded into WPS installation |
| • | Improvements in trend performance |
| • | Improvements in design, icons, windows ... |
| • | Main resource set was simplified |
| • | Menu actions restructured and actions sensitive to the context |
| • | Configuration import with validation of .bkp file |
| • | Alphabetic ordering of configurations and resources |
| • | Support to bitfields in parameters table |
| • | Parameter monitoring inside ladder |
WPS V2.10
Functionalities:
| • | PLC300 v2.30 with support to Hot Download and Watchdog |
| • | Importer/Conversor from WLP Projects to WPS to the equipment SCA06 |
| • | Full impression of configurations and resources |
| • | Variables Monitoring with functionality to backup and restore variables values |
| • | Created window with information about the device connected |
| • | Create window with additional information such author, description and client about the resource |
Improvements:
| • | WPS Help rewriten to all ladder blocks |
| • | Window of variable selection changed to a table format with filter options |
| • | Move variables from one block to another in the ladder editor |
| • | Search of variables with filters |
| • | Support the movement of multiple variables simultaniously in structures and also record of last type added for future additions |
| • | USB Driver with support to Windows 8.1 |
WPS V2.00
Functionalities:
| • | Support to SCA06 starting at firmware version v2.00, agregatting the functios of SuperDrive G2 and WLP |
| • | PLC300 v2.10 with support to Strings |
WPS V1.80
Functionalities:
| • | PLC300 V2.00 Support (Hardware Version 2) |
| • | P_RAMP Block (Pulse Train) |
WPS V1.70
Functionalities:
| • | Upload and download variable data, this function allows to preserve variables values during the program download. This function is compatible with firmware v1.70 or above. |
| • | Export and download binaries |
| • | Creation of "text input" component on screen editor |
Improvements:
| • | Project management: |
| • | Creation of multiple CANopen configurations |
| • | Possibility of association of a ladder to a task on the last wizard step during the new ladder wizard |
| • | Ladder editor: |
| • | Optimization in ladder diagram editor, reducing the use of CPU and memory |
| • | Dragging variable from variables list and dropping it into the block argument |
| • | RUNG title length increased |
| • | Number of elements per RUNG increased |
| • | Automatic tag break |
| • | Screen name display during configuration of F buttons in screen editor |
| • | Optimization in monitoring to reduce the response time |
| • | Optimization in compiler to reduce compile-time |
| • | Clock synchronization between the computer clock and project setup |
Corrections:
| • | Correction during removal of POU from task, where changes are not saved when another action is not made in sequence |
| • | Correction in the compiler when the same POU was linked to more than one task |
| • | Correction of lock during the load of variables table when large structure type is used |
| • | Correction for performance increase during search of structure fields |
| • | When the component "numeric input" was configured as INT and contains decimal digits the limit values were not being compiled correctly |
| • | Unset of main selection during resource version change |
| • | Function keys were not working when used with variables of type BOOL with size bigger than 0 (zero), the compiler was not generating the correct memory address for this variables |
| • | SD Card password was being stored even with the related option disabled, the compiler was not checking the signal of SD Card password |
| • | During compiling errors where the variable does not exist anymore, the compiler was not displaying the variable name |
| • | When two variable nodes of structures were expanded on variables table at the same time one of the structures displays the variables names as ??? |
| • | The variables sampled in event log were not displaying the correct values |
| • | Correction of functional deviation in the compiler when any argument from the USERFB was a member of a structure or an instance. In this case the number of bits that was being considered was the size of the whole structure, when the correct should be only the size of this member |
| • | Correction of functional deviation in the compiler when distinct ladders were calling USERFB instances with the same name, occasionally, the compiler was inverting the call of USERFB's. The compiler was overwriting the arguments file from the USERFB, when the name of instance was the same |
| • | Do not allow creation of folder and files related to USERFB with invalid names |
| • | Block of "text" component editing when it reaches his limit size |
| • | Alarm compilation was not displaying correct variables names in case of compiling errors |
| • | Correction of validation on new task creation |
| • | During compilation in case of duplicated variables the compiler was not displaying the duplicated variable name |
| • | Correction into resource comparison, in specific situations in Ladder files, some small differences are not being detected by the function |
WPS V1.60
Functionalities:
| • | USERFB User Function Block |
| • | Comparison of the resource in the application to a resource of the device |
| • | Download of the device setup and CANopen configuration |
| • | New faster and easy-to-use screen editor |
| • | Options to enable and disable alarms on the editor |
Improvements:
| • | Project management: |
| • | "Save as..." in the resource configuration |
| • | "Search" for the variables in all the resource |
| • | Properties of the resource folder |
| • | Edition of structure members |
| • | Indication in the files open on the editor if they belong to the main selection |
| • | Highlight on the programs not used in any tasks |
| • | Link on the output window of the compiler |
| • | Alarm keys: |
| • | Automatic resizing of the Message component |
| • | Shortcut keys in the alarm edition |
| • | Printing of the screens with their properties |
| • | Ladder editor: |
| • | Allow to change the contact or coil type already inserted in the ladder |
| • | Change of the output variables of the BYTE counters for BOOL to use in contacts |
| • | Variables: |
| • | Possibility to erase multiple variables from the variable window |
| • | Disable the variable window when closing or changing the resource selection |
| • | Selection of the variable address by means of the Modbus address |
Corrections:
| • | Increase of the number of retries before displaying the error messages during the online monitoring |
| • | Correction of fault when saving the renamed variables. After renaming the variables, the save button was not being enabled and the changes were not being saved. |
| • | Change of the default .csv variable importation file from "," to ";". |
| • | Locking of the renaming action in the GLOBAL_IO group. |
| • | Change of the maximum memory area size of the screens |
| • | Compiler presented error when compiling structure with invalid element. Change to accept repeated variables in GLOBAL_IO group. |
| • | 32-bit data types (DWORD, DINT, UDINT, REAL) enabled for the network variables |
| • | Fault in the compilation of the watchdog variables of the start, stop and main tasks |
| • | Fault in the compilation of String variables using the STRING# syntax in the ReadRecipe and WriteRecipe blocks. Correction to generate error in this situation |
| • | Fault when using the STORE block of a REAL variable for a member of a REAL structure |
| • | Correction of a fault when saving the monitoring variables. The new variables created were not being saved. |
| • | Correction of the ordering of the numerical fields in the variable table. .When ordering the table, the numerical fields were not correctly ordered |
| • | Locking of the edition of system variables. It was possible to edit the variable and duplicate it. |
| • | Correction of the fault in the resource exportation. Not all the internal files were being copied. |
| • | Correction of the fault when importing resource with the override option enabled. The configuration was not being overridden correctly. |
| • | Correction to remove the selection edge of the component after copying components on different screens. |
| • | Correction to reduce the memory consumption when loading the screens. |
| • | Problem in the alignment of the structures containing the BOOL data type. It was observed that the monitoring of the BOOL array was presenting incorrect values. |
| • | Correction of the edition of the array of the SDO_Write block. |
WPS V1.50
Functionalities:
| • | Program upload |
| • | Force I/O |
| • | Language configuration in the PLC300 setup |
| • | Option to display variables on the alarm screens |
| • | Option of filling in the fields "Numeric Input" and "Numeric Output" with zeros on the user’s screens |
| • | Download option: |
| • | Initialize output and volatile variables |
| • | Stop/Start the execution of the program automatically |
| • | Online command menu for the password-protected operations of recording and loading program, setup and firmware on the SD card. |
Improvements:
| • | Printing of the ladder diagrams |
Corrections:
| • | Increase the number of retries before displaying the error messages during the online monitoring |
| • | Correction of fault when recording the renamed variables. After renaming the variables, the save button was not being enabled and the changes were not being recorded. |
| • | Change of the default .csv variable import file to ";" instead of ",". |
| • | Locking of the renaming action in the GLOBAL_IO group. |
| • | Change of the maximum memory area size of the screens |
| • | Compiler presented error when compiling the structure with invalid element. Change to accept repeated variables in GLOBAL_IO group. |
| • | 32-bit data types (DWORD, DINT, UDINT, REAL) enabled for the network variables |
| • | Fault in the compilation of the watchdog variables of the start, stop and main tasks |
| • | Fault in the compilation of String variables using the STRING# syntax in the ReadRecipe and WriteRecipe blocks. It was corrected to generate error in this situation |
| • | Fault when using the STORE block of a REAL variable for a member of a REAL structure |
| • | Correction of a fault when recording the monitoring variables. The new variables created were not being recorded |
| • | Correction of the ordering of the numerical fields in the variable table. When ordering the table, the numerical fields were not correctly ordered |
| • | Locking of the system variables edition. It was possible to edit the variable and duplicate it. |
| • | Correction of the fault in the resource export. Not all the internal files were being copied. |
| • | Correction of the fault when importing resource with the override option enabled. The configuration was not being overridden correctly. |
| • | Correction to remove the component selection edge after copying component on different screens. |
| • | Correction to reduce the memory consumption when loading the screens. |
| • | Problem in the alignment of the structures containing the BOOL data type. It was observed that the monitoring of the BOOL array was presenting incorrect values. |
| • | Correction in the edition of the SDO_Write block array. |
WPS V1.40
Functionalities:
| • | WPS translated to english and spanish |
| • | Update center |
Corrections:
| • | Move variables between groups by the ladder editor |
| • | Open modbus file manager |
WPS V1.30
Functionalities:
| • | Ethernet configuration at Setup |
| • | Structure Configuration |
| • | Recipe Configuration |
| • | Event Log Configuration |
| • | Modbus File Manager |
Ladder Editor:
Corrections:
| • | Optimization of the ladder editor so as to guarantee ladder files with up to 200 rungs and moderate memory and CPU consumption. In such situation, the 1.20 version of WPS presented slow performance and crashes. |
PLC300:
| • | New Features and Corrections of PLC300. |
WPS V1.20
| • | Communication with the PLC300 V1.2X equipment, |
| • | Task programming, |
| • | Change in tag addresses for compatibility with Modbus, |
| • | Tool to import/export projects, |
| • | Checking the PLC300 firmware version during download, |
| • | Stop/run programs as global actions, |
| • | Environment persistence when exiting, |
| • | Improvements in communication, |
| • | Download options: |
| o | Initialize retentive variables, |
| o | Clear alarm history, |
| o | Font code download. |