Navigation:  Quick Start >

Firmware Download

Previous pageReturn to chapter overviewNext page

wpshelp_common_fig_note

NOTE!

 

This feature does not allow you to download the firmware directly from the internet.

 

To use it, you will need to obtain the binary file from the supplier/technical support in advance.

 

 
The WPS allows you to update the firmware of some products using the “Firmware Download” feature, which is accessible via the “Online” menu located in the upper left corner.

 

download_firmware_example_01

 

download_firmware_example_02

 

When you click on “Firmware Download,” an interaction panel will appear, allowing you to configure communication with the device.

 

download_firmware_example_03

 

In the “Device” section, select the desired equipment in the “Default” field, configure the corresponding physical layer, and perform the corresponding Communication configuration.

 

Then, use the “Test” button, located next to the “Current connection” field, to verify that communication is working correctly.

 

The result will be displayed in the “Status” field, which should return “Device Online” for the firmware update process to proceed.

 

After obtaining this status, simply click the “Next” button located in the lower right corner of the interaction panel.

 

The update process for each device can be followed through a step-by-step guide available on the “Firmware Download” page, within the specific section for each equipment. Below, you will find a list with specific instructions for each equipment:

 

ADW300
CFW100
CFW300
CFW300-2
CFW320
CFW500
CFW501
CFW503
CFW900
PLC200
PLC300
SCA06
SIW750
SSW900
SSW900-CETH-W
WECC300

 

wpshelp_common_fig_note

NOTE!

 

Additional information can be found at Supported Equipments.