What's New - Previous Versions
WPS V3.00 ## WPS V3.00 ### Features - Included CFW900 V1.00.xx - Included CFW700 v2.3x - Included CFW500 v3.6x - Included CFW300 v3.0x - Included CFW100 v4.1x - Included MW500 v3.0x - Included RUW100 v2.0x - Included WECC300 v1.1x - Included WECC300 v1.2x - Included WCW2200 v2.2x - Included Enterprise v1.0x - Included SIW750 v1.1x - Included SIW700 v2.2x - Included SIW600 v2.6x - Included SIW600 v2.7x - Included MVW-01 v3.0x - Included MVW-01 v3.2x - Included MVW-01 v3.3x - Included MVW-01 v3.4x - Included MVW-01 v3.5x - Included MVW3000 v1.1x - Included MVW3000 v1.2x - Included MVW3000 v1.3x - Included MVW3000 v1.4x - Included SSW7000 v1.1x - Included SSW7000 v1.2x - Included SSW7000 v1.3x - Included SSW7000 v1.4x - Included SSW7000 v1.5x - Included SSW7000 v1.6x - Included SSW7000 v1.7x - Included RTD v2.7x - Included RTDW v1.0x - DriveScan configurator and download for CFW900 - Converter improvement WLP to WPS - Wizard for ECW500 Status - Wizards for PSRW 1.1x - Firmware download for CFW500 - Firmware download for MW500 - Firmware download for WECC300 - Event log for WCW2200 - Parameter export - Show data type in parameter table - Import of device versions (Ve's) - Trend: real sampling rate, pause option, allows monitoring more channels ### Modifications - Trend: correction in zoom adjustment, performance improvement ## WPS V2.60 ### Features - Included ADW300 v1.00+ - Included CFW-05 v1.00+ - Included CFW-07 v2.00+ - Included CFW-08 v1.00+ - Included CFW-09 v1.20+ - Included CFW-09PM v10.00+ - Included CFW-11 v6.00+ - Included CFW-11M-G2 v1.10+ - Included CFW-11RB v1.10+ - Included CFW300 v1.00+ - Included CFW-300-2 v2.00+ - Included CFW700 v1.00+ - Included CFW701 v1.10+ - Included Corporate v1.00+ - Included CTW-04 v1.00+ - Included CTW900 v1.00+ - Included ECW500 v1.00+ - Included FAW700 v1.30+ - Included MVW-01 v1.40+ - Included MVW3000 v1.00+ - Included RUW100 v1.00+ - Included SCA-04 v1.00+ - Included SCA-05 2.10+ - Included SCW100 v1.00+ - Included SIW600 v2.50+ - Included SIW700 v1.80+ - Included SIW750 v1.00+ - Included SSW700 v1.00+ - Included SSW900-CETH-W v1.10 - Included WCW2200 v1.10+ - Included WEC300 v1.00 - Added wizards option - Added Firmware Download - Implemented Trace for MVW3000 - Added ladder blocks: MW_SRAMP and MW_Stop2 - Implemented Force I/O for CFW100 ### Modifications - Improvements in Communication Manager - WComm - Corrections in the manual (help) - Improvements in task compilation - Improved Trace resolution - Added Modbus address in the ladder tooltip - Improved search tool ## WPS V2.50 ### Features - Included CFW500 V1.10+ - Included CFW501 V1.30+ - Included MW500 V1.50+ - Included CFW-11 V1.00+ - Included SSW06 V1.30 - Included SSW07 V1.20 - Included SSW08 V1.30 ### Improvements - Corrections in the manual (help) ## WPS V2.40 ### Features - Configuration Wizard - CFW300, PSRW, SSW900 - Monitoring windows of the main signals - CFW300, SSW900 - CALL block for PLC300 from versions V3.41 and V4.11 (according to the hardware model) - USB driver for communication with PSRW - Improved search system (includes search by blocks, indexed variables, texts) ### Improvements - Corrections in the manual (help) - WComm (communication manager with FTP support) - WEG USB driver with Windows support 10 (x86 and x64) - including build 1607 or later - New marker addresses for HMI LED configuration (PLC300 V4.1X) ## WPS V2.30 ### Features - Included CFW300 V1.0X and V1.2X - Included PLC300 V3.3X - Support for Windows 10 (x86 and x64) - Automatic installation of WEG USB driver - Automatic installation of FTDI driver - Welcome window with quick access to some functions - Improved communication configuration ### Improvements - Improved trend graph performance and interface - Improved menu organization ## WPS V2.20 ### Features - Function to remove unused variables - Function to search and replace variables in the resource - Variable filter in the variable table ### Improvements - JRE (Java) built into the WPS installation - Improvements in trend performance - Improvements in design, icons, windows, etc. - Simplified main resource definition - Restructuring of menu actions and context-sensitive actions - Configuration import with .bkp file validation - Sorting of settings and resources alphabetically - Support for bitfields in the parameter table - Monitoring of parameters in the ladder ## WPS V2.10 ### Features - PLC300 v2.30 with Hot Download and Watchdog support - Importer/Converter of projects from WLP to WPS for the SCA06 equipment - Complete printing of settings and resources - Monitoring of variables with functionality to backup and restore the values of variables - Created screen with information of the connected device - Created screen for additional information of the resource such as author, description and client ### Improvements - WPS Help rewritten for all ladder blocks - Variable selection window changed to table format with filter options - Move variables from one block to another in the ladder editor - Search for variables with filters - In the structures section, support was added for moving several variables simultaneously and remembering the last data type added for future additions - USB driver with support for Windows 8.1 ## WPS V2.00 ### Features - Support for SCA06 from firmware version v2.00, adding the functions of the SuperDrive G2 and WLP software - PLC300 v2.10 with support for Strings ## WPS V1.80 ### Features - PLC300 V2.00 (Hardware version 2) - P_RAMP block (generates pulse train with frequency ramp) ## WPS V1.70 ### Features - Upload and download of variable data, allowing to preserve the value of the variables during program download. Compatible with firmware v1.70 or higher - Export and download of binaries - Creation of a Text Input type component in the screen editor ### Improvements - Project management: - Creation of multiple CANopen configurations - Possibility of associating the Ladder to a task in the last step of its creation in the wizard - Ladder Editor: - Optimization in the Ladder diagram editor, reducing processor and memory usage - Drag 'n drop of variables from the variable list to the block arguments - Increased rung title size - Increased number of elements per rung - Automatic wrapping of tags - Display of screen names when configuring a function button to call a screen - Optimization in monitoring to reduce response time - Optimization in the compiler to reduce compilation time - Option to synchronize the clock with the computer's clock in setup ### Fixes - Correction during deletion of the POU from the task, where the changes were not saved if another action was not performed later - Correction in the compiler when the same POU was associated with more than one task - Fixed a fix during loading of the variable table, which would crash when associated with a very large structure type. - Fixed an issue to increase performance when searching for structure fields. - When the Numeric Input component was configured as an integer and contained decimal digits, the limit values were not being compiled correctly. - Loss of the main selection when changing the device version. - Function keys did not work when used with BOOL variables with a size greater than 0 (zero). The compiler was not generating the correct memory address to access BOOL variables with a size greater than 0 (zero). - The SD card password was being saved when the option was disabled; the compiler was not checking the SD card password enable flag. - In compilation errors where the variable no longer exists, the compiler did not display the variable name. - When two variable structure nodes were expanded in the variable table at the same time, one of the structures displayed the variable name as ??? - The variables sampled in the event log were not displaying their values correctly. - Fixed a functional error in the compiler when any argument of a USERFB was a member of a structure or instance. In this case, the number of bits being considered was the size of the entire structure, when the correct number should be only the size of this member. - Fixed a functional error in the compiler when there were different Ladder files calling USERFB with instances with the same name. Occasionally, the compiler would invert the USERFB calls. It was overwriting the USERFB argument file, when the name of the USERFB instance was the same, being in different files - Do not allow creation of folders and files related to USERFB with invalid names - Blocking in editing the Text component when it reaches its size limit - When compiling alarms, wrong variable names were displayed in case of error - Fixed validation when creating a new task - Fixed during compilation in case of duplicate variables: the compiler did not display the name of the duplicate variable - Fixed in the comparison resource: the Ladder files were not being compared correctly, in specific situations there were small divergences that were not identified ## WPS V1.60 ### Features - USERFB user block - Comparison of the resource in the application with the device resource - Download of the device setup and CANopen configuration - New screen editor, faster and easier to use - Options to enable and disable alarms in the editor ### Improvements - Project management: - Save as... in configuration and resource - Search for variables in the entire resource - Resource folder properties - Editing structure members - Indication in files open in the editor to indicate if they belong to the main selection - Highlighting in programs not used in any task - Link in the compiler output window - Screens and alarms: - Automatic resizing of the Message component - Shortcut keys when editing alarms - Printing screens with their properties - Ladder Editor: - Allow changing contact or coil types already inserted in the Ladder - Changing counter output variables from BYTE to BOOL for use in contacts - Possibility of deleting multiple variables from the variables window - Disable the variables window when closing or changing resource selection - Selection of the variable address through the Modbus address ### Corrections - Increased number of retries before displaying error messages during online monitoring - Fixed failure when saving renamed variables. After renaming variables, the save button was not being enabled and changes were not being saved. - Changed the default .csv variable import file to ; instead of , - Blocked the rename action in the GLOBAL_IO group. - Changed the size of the maximum memory area for screens. - The compiler presented an error when compiling a structure with an invalid element. - Changed to accept repeated variables in the GLOBAL_IO group. - Enabled 32-bit data types (DWORD, DINT, UDINT, REAL) for network variables. - Failure to compile watchdog variables for Start, Stop, and Main tasks. - Failure to compile String variables using the STRING# syntax in the ReadRecipe and WriteRecipe blocks. It has been fixed to generate an error in this situation. - Failure to use the STORE block of a REAL variable for a member of a REAL structure. - Fixed a failure to save monitoring variables. Newly created variables were not being saved. - Fixed the ordering of numeric fields in the variables table. When sorting the table column, the numeric fields were not sorted correctly. - Blocked editing of system variables. It was possible to edit the variable and duplicate it. - Fixed a bug when exporting the resource. Not all internal files were being copied. - Fixed a bug when importing a resource with the overwrite option enabled. The configuration was not being overwritten correctly. - Fixed removing the component selection border after copying the component to different screens. - Fixed reducing memory consumption when loading screens. - Issue with the alignment of structures containing the BOOL data type. It was observed that the BOOL array monitoring was showing incorrect values - Fixed editing of the SDO_Write block array ## WPS V1.50 ### Features - Program upload - Force I/O - PLC300 language configuration in setup - Option to present variables on alarm screens - Option to fill with zeros in the Numeric Input and Numeric Output fields on user screens - Download option: - Initialize volatile and output variables - Stop/Start program execution automatically - Online command menu for saving and loading the program, setup and firmware on the SD card, password protected. ### Improvements - Printing of Ladder diagrams ### Corrections - Increased number of retries before displaying error messages during online monitoring - Fixed failure when saving renamed variables. After renaming variables, the save button was not being enabled and the changes were not being saved. - Changed the default .csv variable import file to ; instead of ,. - Blocked the rename action in the GLOBAL_IO group. - Changed the size of the maximum memory area of screens. - The compiler presented an error when compiling a structure with an invalid element. - Changed to accept repeated variables in the GLOBAL_IO group. - Enabled 32-bit data types (DWORD, DINT, UDINT, REAL) for network variables. - Failure to compile watchdog variables for Start, Stop, and Main tasks. - Failure to compile String variables using the STRING# syntax in the ReadRecipe and WriteRecipe blocks. It has been fixed to generate an error in this situation. - Failure to use the STORE block of a REAL variable for a member of a REAL structure. - Fixed the failure to save monitoring variables. Newly created variables were not being saved. - Fixed the ordering of numeric fields in the variables table. When sorting the table column, the numeric fields were not sorted correctly. - Blocked editing of system variables. It was possible to edit the variable and duplicate it. - Fixed a bug when exporting the resource. Not all internal files were being copied. - Fixed a bug when importing a resource with the overwrite option enabled. The configuration was not being overwritten correctly. - Fixed removing the component selection border after copying the component to different screens. - Fixed reducing memory consumption when loading screens. - Issue with the alignment of structures containing the BOOL data type. It was observed that the BOOL array monitoring was showing incorrect values - Correction of the SDO_Write block array editing ## WPS V1.40 ### Features - WPS translated into English and Spanish - Update Center ### Fixes - Move variables between groups using the Ladder editor - Open Modbus file manager ## WPS V1.30 ### Features - Variable Editor Update - Ethernet configuration in setup - Structures configuration - Recipes configuration - Event Log configuration - Modbus File Manager - Ladder Editor: - Workspace Changes - Use of Literals - Use of Arrays - Use of Instances and Structures - Optional Arguments for Function Blocks - New Copy/Paste Features - New Online Monitoring Features ### Fixes - Ladder editor optimization to guarantee Ladder files with up to 200 rungs and moderate memory and CPU consumption. In WPS version 1.20, in this situation, slowness and crashes occurred ## PLC300 - PLC300 News and Fixes. ## WPS V1.20- Communication with PLC300 V1.2X equipment - Task programming - Change in marker addresses for compatibility with Modbus - Tool to import/export projects - Checking the PLC300 firmware version when downloading - Stop/run program as a global action - Environment persistence when exiting - Communication improvements - Download options: - Initialize retentive variables - Clear alarm history - Source code download.