Skip to main content

Installing

When installing a newer version of WPS, it is recommended that you first remove the previous version and reboot the system to ensure the new installation runs correctly.

Close all running programs to avoid interfering with the installation process and follow the steps described below.

  1. Double-click the installer icon to launch the installer. The installation program will start and a welcome window will appear.
  2. In the installation wizard, respond to the License Agreement, then press the Next button.
  3. Specify an empty folder in which to install WPS v3.1X. Ensure the installation location is correct and that there is sufficient disk space for the installation.
  4. Confirm to create an empty folder.
  5. Select the desired installation type.
  6. Select the program group to create the WPS v3.1X shortcuts.
  7. Select additional program shortcuts: create a desktop shortcut and create a quick launch shortcut.
  8. Click the Install button to begin the installation.
  9. Click the Finish button to complete the setup.