Navigation:  Communication >

USB Cables

Previous pageReturn to chapter overviewNext page

The figure below details the cable for the point-to-point USB connection.

 

Figure 1: USB Cables

Figure 1: USB Cables

 

The figure below shows the connectors.

Figure 2: USB Connectors

Figure 2: USB Connectors

 

A = Type A Connector

B = Type B Connector

mini-B = Type mini-B Connector

C = Type C Connector

 

Maximum cable size: 3 meters.

 

wpscommunicationsupport_common_fig_note

NOTE!

Always use a USB shielded interconnection cable, standard host/device shielded USB cable. Unshielded cables may generate communication errors.

 

wpscommunicationsupport_common_fig_note

NOTE!

The USB connection is galvanically isolated from the power grid and other elevated voltages internal to the drive. The USB connection, though, is not isolated from the protection earthing (PE). Use an isolated laptop to connect to the USB connector, or a desktop connected to the same protection earthing (PE) as the drive.