Navigation:  Equipments (Devices) > PLC300 > Communication >

Modbus File Manager

Previous pageReturn to chapter overviewNext page

Overview

 

The modbus file manager of the PLC300 is accessed through the communication menu as shown in the following figure.

 

modbusfilemanager_fig1

 

The window of the modbus file manager is composed of the following parts as shown in the following figure.

 

1.Toolbar with all the tools of the file manager.
2.Folder list of the SD Card.
3.File list of the selected folder.

 

modbusfilemanager_fig2

It is only possible to view the files and folders of the SD Card when the WPS is connected to the PLC300 through the command Connect Device modbusfilemanager_fig13 .

 

 

Toolbar

 

modbusfilemanager_fig3 Creates a new folder

modbusfilemanager_fig4 Erases the selected folder

modbusfilemanager_fig5 Renames the selected folder

modbusfilemanager_fig6 Erases the selected file

modbusfilemanager_fig7 Displays the properties of the selected file (path, size and date)

modbusfilemanager_fig8 Renames the selected file

modbusfilemanager_fig9 Sends the file to the PLC300

modbusfilemanager_fig10 Receives the selected file from the PLC300

 

 

Popup menu

 

In order to access the popup menu, just click the right button on a folder or on a file and it will be displayed as shown in the following figure.

 

Popup menu for folders:

 

modbusfilemanager_fig11

 

Popup menu for files:

 

modbusfilemanager_fig12