Navigation:  Programming > Variables >

Overview

Previous pageReturn to chapter overviewNext page

During the Ladder edition, it is necessary to define the variables used in the Ladder components. This definition can be done directly in the Ladder and/or in the editor/list of variables.

 

The table of variables must be activated through the menu Window > Variables as shown in the following figure.

 

wpshelp_ladder_editor_var_fig4

 

In the variable edition window, the following commands are available:

 

wpshelp_common_fig_plus_sign - Add a new variable

wpshelp_common_fig_edit - Edit the selected variable

wpshelp_common_fig_minus_sign - Remove the selected variable

wpshelp_common_fig_moveup - Move the selected variable one row up in the table

wpshelp_common_fig_movedown - Move the selected variable one row down in the table

wpshelp_common_fig_renamevariable - Rename the selected variable

wpshelp_common_fig_table_export - Export variables from this group to a file

wpshelp_common_fig_table_import - Import variables to this group from a file

 

The variables of the GLOBAL scope (1) present the groups (2) as shown in figure 1.

 

Figure 1: Variable Editor for the "GLOBAL" Scope

Figure 1: Variable Editor for the "GLOBAL" Scope

 

In this area of the global variables, the following groups are available:

 

Constant: variables that store constant values
Global: variables accessible by all the Ladder files
Global Retentive: similar to the global group, but with retentive memory
System Global: variables previously defined with system functions
Global Parameter: variables from device accessible by Ladder and HMI
I/O Global: physical inputs and outputs of the equipment
Network Global: Variables previously defined for network communication

 

The variables of the LOCAL scope (1) present the groups (2) as per figure 2.

 

Figure 2: Variable Editor for the "LOCAL" Scope

Figure 2: Variable Editor for the "LOCAL" Scope

 

In this area of local variables, the following groups are available:

 

Location: variables only accessible through the Ladder that is being edited
Local Retentive: similar to the local group, but with retentive memory

 

wpshelp_common_fig_note

NOTE!

A retentive memory keeps its value even with the equipment off.