Navigation:  Equipments (Devices) > RTD > Parameters >

Read and Write of Parameters

Previous pageReturn to chapter overviewNext page

There are 3 (three) ways to do the reading and writing of the parameters: by means of table, selection and group.

 

1. Table writing. The table writing command will send all visible parameters on the equipment screen. If and error occurs during the sending of some specific parameter, a message will be shown on the output window informing the error. It is important to notice that only visible parameters will be sent; therefore, it is necessary attention to which node of the group of parameters tree you are viewing. Example: If you wish to write all of them without filtering per group, just select the tree root.

 

xmlparametersfilesupport_img_06

 

 

2. Table reading. The table reading command will read all the parameters of the equipment. If a error occurs during the reading of some specific parameter, a message will be shown on the output window informing the error. It is important to notice that only visible parameters will be read; therefore, it is necessary attention to which node of the group of parameters tree you are viewing. Example: If you wish to read all of them without filtering per group, just select the tree root.
 

 

xmlparametersfilesupport_img_07

 

3. Reading/writing of specific parameters. In order to read/write one or more specific parameters, just select them on the table, right click and choose the desired option: read or write parameter.
 

xmlparametersfilesupport_img_08

 

4. Reading/writing of group of parameters. In order to read/write only one group of parameters, just select it on the group tree, right click and choose the desired option: read or write group.

 

xmlparametersfilesupport_img_09