Navigation:  Equipments (Devices) > RTD > Diagnostic > Log >

Overview

Previous pageReturn to chapter overviewNext page

The log function allows viewing the present alarms/faults and also the last alarms/faults in a more friendly and centralized way than on the equipment HMI, showing the data in tabular form.

 

All downloaded alarms/faults are saved in a file in order to keep a record for future reference; it is also possible to export the saved data as a csv file.

 

Below is an overview of the SCA06 log table.

 

xmllogsfilesupport_geral_fig1

 

1.Actions. Below is the sequential description of each action:
1.1.On-Line Reading: This action constantly searches for new faults/alarms on the equipment; in case any occurs, the table is automatically updated.
1.2.Read Logs: This action reads all faults/alarms only once and updates the table.
1.3.Export: Export of data shown in the table as a CSV file.
2.Present Fault and Alarm. This field shows the present fault and alarm of the equipment if present; otherwise, the OK message is shown.
3.Fault and Alarm Table. This table shows all the faults and alarms, as well as the date when they occurred, code and description.