Skip to main content

Why Can I Not Update the CFW500 Firmware?

A CFW500 firmware update depends on the communication settings used by WPS and by the device. If these settings are not compatible with the firmware download procedure, WPS may fail to start the update or may not detect the device correctly.

What to Check First

Before starting the firmware update, verify the following items:

  1. WPS is updated and the CFW500 device module is installed.
  2. The communication cable and interface are connected correctly.
  3. The serial port selected in WPS is the port used by the device.
  4. The baud rate and other communication settings match the firmware download procedure described in the CFW500 manual.
  5. The device remains powered during the entire update.
  6. No other software is using the same communication port.
caution

Do not interrupt power or disconnect the communication cable during a firmware update. An interrupted update may require a recovery procedure.

Where to Find the Detailed Procedure

The detailed CFW500 firmware download procedure is available in the WPS manual at:

Devices > CFW500 > Firmware Download

Use that section as the reference for the required baud rate, serial port, and product-specific instructions.

  1. Confirm that WPS can communicate with the CFW500 before starting the firmware update.
  2. Check the serial port and baud rate required by the firmware download procedure.
  3. Close any other program that may be using the same communication port.
  4. Restart WPS and try the firmware download again.
  5. If the device is still not detected, review the physical connection and the communication interface.

Expected Result

WPS detects the CFW500 using the required communication settings and starts the firmware download procedure.