Skip to main content

PTSCONTACT

PTSCONTACT is a rising-edge transition contact used in Ladder logic.

Ladder representation​

PTSCONTACT ladder representation

Block structure​

Variable TypeNameData TypeDescription
VAR_INPUTI1BOOLBlock control input.
VARPTSCONTACT_INST_0PTSCONTACTBlock structure access instance.

Operation​

When variable I1 transitions from FALSE to TRUE (rising edge or positive transition edge), B receives the value of A for one scan cycle. At all other moments, B receives FALSE.

Series And Parallel Associations

Pay attention to series and parallel contact associations. See the Contact Logic section for more information.

Logic diagram​

PTSCONTACT logic diagram

Execution flowchart​

PTSCONTACT execution flowchart

Examples​

PTSCONTACT ladder example

In this example, digital output DO1 is reset when the SHIFT key is pressed and a positive pulse is detected at digital input DI2.