Navigation:  Quick Start >

New Configuration - Online Equipment

Previous pageReturn to chapter overviewNext page

In the following example, we will create a configuration with the CFW300. The windows may be different if other equipments are configured.

 

 

CFW300

 

 

1) New Configuration Menu Item/Button

 

In the File menu, click New Configuration.

 

wpshelp_quick_start_create_new_configuration-online-01a

 
You can also use the keyboard shortcut (Ctrl+Shift+C) or the New Configuration button on the Toolbar: wpshelp_quick_start_create_new_configuration-online-01b

 

 

2) New Configuration Window

 

A window will pop up prompting you to enter the configuration name and the first resource to be created. Enter the names in the respective fields and click Next.

 

wpshelp_quick_start_create_new_configuration-online-02

 

wpshelp_common_fig_note

NOTE!

This window allows you to create a Resource or an Application.

Applications are restricted to specific product versions.

Please consult equipment´s manual for more information about Applications.

 

 

3) Communication Configuration

 

The next window defines the options for communication with the equipment.

 

wpshelp_quick_start_create_new_configuration-online-03

 

 

4) Select the Communication Options

 

Choose the correct communication options.

 

If you select one equipment, the default configuration of the communication of the equipment will be loaded to the window.

 

Still, check that the window configuration is the same as of the equipment. If not, update this window according to the equipment configuration.

 

wpshelp_quick_start_create_new_configuration-online-04

 

 

wpshelp_common_fig_note

NOTE!

In this example, the CFW300-CUSB accessory is being used, which appears in Windows as a USB serial port (virtual COM port);
When the cable is connected to the personal computer/equipment, the Windows device manager informs the name of the USB serial port which was created.

 

 

5) Testing the Communication

 

You can check if the communication is correct by clicking the Test button in this window.

 

The status field is refreshed. The connected equipment appears in the status field.

 

wpshelp_quick_start_create_new_configuration-online-05

 

Then click Next.

 

 

6) Equipment Selection

 

The window shows the equipment that is connected to the resource that was created.

 

wpshelp_quick_start_create_new_configuration-online-06

 

 

7) Read ID

 

If you click the Read ID button, a window containing the information on the equipment will open. Click OK to close it.

 

wpshelp_quick_start_create_new_configuration-online-07

 

In order to go to the next step, click Next.

 

 

8) Import from WLP

 

A new window pops up enabling to import from the CFW100 a Ladder project developed on the WLP (WEG Ladder Programmer).

 

wpshelp_quick_start_create_new_configuration-online-08

 

 

Click Finish to close the wizard.

 

 

9) Configuration Tree

 

After those steps, the tree with the configurations should look like the following image.

 

wpshelp_quick_start_create_new_configuration-online-09

 

 

10) Resource Properties

 

The settings made in the setup can be changed later in resource properties.

 

wpshelp_quick_start_create_new_configuration-online-10

 

 

wpshelp_common_fig_note

NOTE!

Depending on the equipment, new windows may appear from this step on, with initial settings and oriented start-ups.