Navigation:  Installation/Uninstallation >

Installing

Previous pageReturn to chapter overviewNext page

When installing a newer version of WPS it is recommended that the previous version be removed first and the system be rebooted, to make sure that the new installation is performed correctly.

 

Close all running programs to avoid interference with the installation process and follow the steps below.

 

1.Double-click the installer icon to start the installer. The installation program will start and a welcome window will appear.
2.In the installation wizard, respond to the License Agreement, then press Next button.
3.Specify an empty folder inside which the WPS v3.1X will be installed. Make sure the installation location is correct and that there is sufficient disk space for installation.
4.Confirm to create an empty folder.
5.Select the type of installation you want.
6.Select the program group to create the shortcuts for the WPS v3.1X.
7.Select shortcuts for additional programs: create a shortcut on the desktop and create a shortcut for quick start.
8.Click the Install button to start installation.
9.Click the Finish button to complete the setup.